Connect to Instruments

The Keysight Instrument Discovery Service auto-discovers many instruments that are physically connected to your PC or are on your local LAN subnet, and automatically adds them to the Instrument list. In some cases, however, you may need to manually add that instrument to your configuration. (For more information, see Troubleshoot Instrument Connections).

Refer to Instrument Configuration on how to configure and validate the connection of instruments.

See Also

Troubleshoot Instrument Connections